All trademarks are the property of their respective owners.
The Texas Instruments LDC211x and LDC3114 devices can monitor changes in a sensor resonant frequency to determine whether a stimuli corresponds to a user interaction such as a button press. Refer to the Inductive Touch System Design Guide for HMI Button Applications application report for details on how to construct a mechanical system suitable for inductive sensing button applications, sensor design guidance, and an overview of device configuration. The LDC211x and LDC3114 use several internal algorithms to compensate for environmental shifts, determine whether the sensor signal change corresponds to a button press, and also to correct for mechanical cross-talk between multiple buttons. This document details the operation and configuration of the algorithms.