SNOA993A June 2018 – July 2021 LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
The LDC211x and the LDC3114 operate in one of two modes – Low Power Mode and Normal Power Mode. In Low Power Mode, the maximum supported scan rate is from 0.625 to 5 sps. In Normal Power Mode, the scan rate is 10 to 80 sps. The primary difference between the two modes is the Baseline Increment, which is discussed below. The buttons enabled in Low Power Mode must be a subset of the buttons enabled in Normal Power Mode.