SNOAA79 June 2021 DAC121S101QML-SP , LMP7704-SP , TPS7A4501-SP
Compliance Voltage
The following figure shows where the circuit saturates as the load resistance is varied. The maximum supported load is 22.47Ω which is almost exactly as anticipated by the previous maximum load calculation.