SNOK010 November 2024 TPS7H6005-SEP
During the SEB/SEGR characterization, the device was tested at room temperature of approximately 25°C. The device was tested under both the enabled and disabled mode. For the SEB-OFF mode the device was disabled using the EN-pin by forcing 0V while in PWM mode and by holding both inputs low during the IIM mode testing. During the SEB/SEGR testing with the device enabled or disabled, not a single input current event was observed.
The species used for the SEB testing was Xenon (129Xe at 25MeV/nucleon) at MSU or Silver (109Ag at 15MeV/nucleon) at TAMU. An angle of incidence of 0° was used to achieve an LETEFF = 50.5MeV×cm2/mg or 48MeV×cm2/mg respectively (for more details, see Ion LETEFF, Depth, and Range in Silicon). The kinetic energy in the vacuum for this ions is 3.225Gev or 1.634GeV respectively. Flux of approximately 105 ions / cm2×s and a fluence of approximately 107 ions/cm2 per run was used. Run duration to achieve this fluence was approximately two minutes. The twelve devices (same as used in SEL testing) were powered up and exposed to the heavy-ions using the maximum recommended input voltage and boot voltage of 14V. The ASW (High-Side Driver Signal Return) was set to 14, 45 or 150 V depending on the variant being tested. The device was set in both PWM and IIM modes during testing. For more information, see Single-Event Effects section. No SEB/SEGR current events were observed during the twenty-six runs, indicating that the TPS7H60x5-SEP is SEB/SEGR-free up to LETEFF = 50.5 MeV×cm2/mg and across the full electrical specifications. Summary of TPS7H60x5-SEP SEB/SEGR Test Condition and Results shows the SEB/SEGR test conditions and results.
Run Number | Unit Number | Variant | Ion | LETEFF (MeV × cm2 / mg) | Flux (ions × cm2/ mg) | Fluence (number of ions) | Enabled Status | VIN | VBOOT | Mode | Switching Frequency | SEB Event? |
---|---|---|---|---|---|---|---|---|---|---|---|---|
15 | 1 | TPS7H6005 | 129Xe | 50.5 | 8.51 × 104 | 1 × 107 | EN | 14 | 14 | PWM | 500kHz | No |
16 | 1 | TPS7H6005 | 129Xe | 50.5 | 8.55 × 104 | 1 × 107 | EN | 14 | 14 | PWM | 1MHz | No |
17 | 1 | TPS7H6005 | 129Xe | 50.5 | 8.36 × 104 | 1 × 107 | EN | 14 | 14 | PWM | 2MHz | No |
18 | 1 | TPS7H6005 | 129Xe | 50.5 | 9.51 × 104 | 1 × 107 | DIS | 14 | 14 | PWM | N/A | No |
19 | 2 | TPS7H6005 | 129Xe | 50.5 | 9.83 × 104 | 1 × 107 | EN | 14 | 14 | IIMENSW | 500kHz | No |
20 | 2 | TPS7H6005 | 129Xe | 50.5 | 8.5× 104 | 1 × 107 | EN | 14 | 14 | IIMENST | N/A | No |
21 | 2 | TPS7H6005 | 129Xe | 50.5 | 1.09 × 105 | 1 × 107 | EN | 14 | 14 | IIMENST | N/A | No |
22 | 2 | TPS7H6005 | 129Xe | 50.5 | 1.08 × 105 | 1 × 107 | DIS | 14 | 14 | IIMENST | N/A | No |
23 | 3 | TPS7H6005 | 129Xe | 50.5 | 1.07 × 105 | 1 × 107 | EN | 14 | 14 | IIMDISSW | 500kHz | No |
24 | 3 | TPS7H6005 | 129Xe | 50.5 | 1.14 × 105 | 1 × 107 | EN | 14 | 14 | IIMDISST | N/A | No |
25 | 3 | TPS7H6005 | 129Xe | 50.5 | 1.11 × 105 | 1 × 107 | EN | 14 | 14 | IIMDISST | N/A | No |
26 | 3 | TPS7H6005 | 129Xe | 50.5 | 1.09 × 105 | 1 × 107 | DIS | 14 | 14 | IIMDISST | N/A | No |
27 | 4 | TPS7H6015 | 129Xe | 50.5 | 1.11 × 105 | 1 × 107 | EN | 14 | 14 | PWM | 500kHz | No |
28 | 4 | TPS7H6015 | 129Xe | 50.5 | 1.14 × 105 | 1 × 107 | DIS | 14 | 14 | PWM | N/A | No |
29 | 5 | TPS7H6015 | 129Xe | 50.5 | 1.12 × 105 | 1 × 107 | EN | 14 | 14 | IIMENSW | 500kHz | No |
30 | 6 | TPS7H6015 | 129Xe | 50.5 | 9.93 × 104 | 1 × 107 | EN | 14 | 14 | IIMDISSW | 500kHz | No |
31 | 7 | TPS7H6025 | 129Xe | 50.5 | 1 × 105 | 1 × 107 | EN | 14 | 14 | PWM | 500kHz | No |
32 | 7 | TPS7H6025 | 129Xe | 50.5 | 1.02 × 105 | 1 × 107 | DIS | 14 | 14 | PWM | N/A | No |
33 | 8 | TPS7H6025 | 129Xe | 50.5 | 1.1 × 105 | 1 × 107 | EN | 14 | 14 | IIMENSW | 500kHz | No |
34 | 9 | TPS7H6005 | 109Ag | 48 | 1.04 × 105 | 1 × 107 | EN | 14 | 14 | PWM | 500kHz | No |
35 | 9 | TPS7H6005 | 109Ag | 48 | 1.1 × 105 | 1 × 107 | DIS | 14 | 14 | PWM | N/A | No |
36 | 10 | TPS7H6015 | 109Ag | 48 | 1.05 × 105 | 1 × 107 | EN | 14 | 14 | PWM | 500kHz | No |
37 | 10 | TPS7H6015 | 109Ag | 48 | 1.08 × 105 | 1 × 107 | DIS | 14 | 14 | PWM | N/A | No |
38 | 11 | TPS7H6025 | 109Ag | 48 | 1.05 × 105 | 1 × 107 | EN | 14 | 14 | PWM | 500kHz | No |
39 | 11 | TPS7H6025 | 109Ag | 48 | 1.06 × 105 | 1 × 107 | DIS | 14 | 14 | PWM | N/A | No |
40 | 12 | TPS7H6025 | 109Ag | 48 | 1.07 × 105 | 1 × 107 | EN | 14 | 14 | IIMDISSW | 500kHz | No |
Using the MFTF method described in Single-Event Effects (SEE) Confidence Interval Calculations, the upper-bound cross-section (using a 95% confidence level) is calculated as: