SNOU206 October 2024 LMG2640
There is an option to disable the PWM input to the daughter card in the event of a fault signal from the LMG2640EVM-090. When the FAULT Protect jumper is placed in the EN mode, PWM is disabled when LMG2640 has an active fault. This disable is not latching, so PWM immediately resumes when the fault clears. If the FAULT Protect mode is not desired, then that mode can be disabled by placing the jumper in the DIS position. The FAULT LED still illuminates when either LMG2640 has an active fault, regardless of the position of FAULT Protect jumper.