Always follow TI’s set-up and application
instructions, including the use of all interface components within the recommended
electrical rated voltage and power limits. Always use electrical safety precautions to
help ensure your personal safety and the safety of those working around you. Contact TI’s
Product Information Center at http://support/ti./com for further information.
Note:
Save all warnings and instructions
for future reference.
Failure
to follow warnings and instructions can result in personal injury, property damage,
or death due to electrical shock and/or burn hazards.
The term TI HV EVM refers to an electronic
device typically provided as an open framed, unenclosed PCB (printed circuit board)
assembly. It is intended strictly for use in development laboratory environments, solely
for qualified professional users having training, expertise, and knowledge of electrical
safety risks in development and application of high-voltage electrical circuits. Any other
use or application is strictly prohibited by Texas Instruments. If you are not suitably
qualified, you must immediately stop from further use of the HV EVM.
- Work Area Safety:
- Maintain a clean and orderly work area.
- Qualified observers must be present anytime circuits are
energized.
- Effective barriers and signage must be present in the area where
the TI HV EVM and the interface electronics are energized; indicating operation of
accessible high voltages can be present for the purpose of protecting inadvertent
access.
- All interface circuits, power supplies, evaluation modules,
instruments, meters, scopes, and other related apparatus used in a development
environment exceeding 50 VRMS/75 VDC must be electrically located within a protected
Emergency Power Off (EPO) power strip.
- Use a stable and non-conductive work surface.
- Use adequately insulated clamps and wires to attach measurement
probes and instruments. No freehand testing whenever possible.
- Electrical Safety:
- As a precautionary measure, a good engineering practice to assume
that the entire EVM can have fully accessible and active high voltages.
- De-energize the TI HV EVM and all the inputs, outputs, and
electrical loads before performing any electrical or other diagnostic measurements.
Confirm that TI HV EVM power has been safely de-energized.
- After confirming the EVM is de-energized, proceed with the
required electrical circuit configurations, wiring, measurement equipment hook-ups,
and other application needs while still assuming the EVM circuit and measuring
instruments are electrically live.
- When EVM readiness is complete, energize the EVM as
intended.
WARNING:
While the EVM is energized, never
touch the EVM or the electrical circuits as the EVM or the electrical circuits can
be at high voltages capable of causing electrical shock hazard.
- Personal Safety:
- Wear personal protective equipment like latex gloves and safety
glasses with side shields, or protect the EVM from accidental touch in an adequate
translucent plastic box with interlocks.
- Limitation for Safe Use:
- EVMs are not to be used as all or part of a production unit.