SNVA057D August 2002 – February 2022 LM2727 , LM2737
The default circuit that comes with the LM2727 demo board uses a bootstrap diode and small capacitor (D1 and CBOOT) to provide enough gate-to-source voltage on the high-side MOSFET to drive the FET. If a separate rail is available that is more than twice the value of VIN, this higher voltage can be connected directly to the BOOT pin, through the BOOT connector, with a 0.1-µF bypass capacitor, CC. In this case, D1 and CBOOT should be removed from the board. Do not connect both CC and CBOOT/D1 at the same time.