SNVA991 October 2022 LM5123-Q1
Type II compensation network is adequate to stabilize the control loop for a peak current mode architecture. A generic technique for selecting the crossover frequency and placement of the error amplifier the pole and zero resulting in a stable system in CCM is presented. The detailed models of the control loop are presented in Section 4. The following section guides the reader through the process of selecting the control loop compensation components; RCOMP, CCOMP and CHF as shown in Figure 2-5. Figure 2-6 shows the type II response of the compensation network. GMea and RCOMP sets the mid band gain (gMID) of the compensation network. The zero frequency fZea is set by the combination RCOMP and CCOMP. The pole is set by the combination of RCOMP and CHF.