SNVAA31 November 2021 LM61435-Q1 , LM61440-Q1 , LM61460-Q1 , LM62435-Q1 , LM62440-Q1
All trademarks are the property of their respective owners.
Figure 1-1 highlights the key differences in device pin-out between the LM614xx and LM624xx device set using the LM61440-Q1 and LM62440-Q1 as device examples.
The primary distinctions between the LM614xx and LM624xx are listed below:
Table 1-1 and Table 1-2 show the device comparison table of the LM61440-Q1 and LM62440-Q1 example devices and illustrates the difference between a LM614xx and LM624xx. The table provides the orderable device numbers and details the variety of different options the device is factory set to. Figure 1-2 and Figure 1-3 are example application circuits from the data sheet. To create a universal footprint to interchange between the LM614xx and LM624xx device set, several components must be considered.
DEVICE | ORDERABLE PART NUMBER | REFERENCE PART NUMBER | LIGHT LOAD MODE | SPREAD SPECTRUM | OUTPUT VOLTAGE | SWITCHING FREQUENCY |
---|---|---|---|---|---|---|
LM61440-Q1 | LM61440AANQRJRRQ1 | LM61440AAN-Q1 | Auto Mode | No | Adjustable | Adjustable |
LM61440AASQRJRRQ1 | LM61440AAS-Q1 | Auto Mode | Yes | Adjustable | Adjustable | |
LM61440AFSQRJRRQ1 | LM61440AFS-Q1 | FPWM | Yes | Adjustable | Adjustable |
DEVICE | ORDERABLE PART NUMBER | REFERENCE PART NUMBER | LIGHT LOAD MODE | SPREAD SPECTRUM | OUTPUT VOLTAGE | SWITCHING FREQUENCY |
---|---|---|---|---|---|---|
LM62440-Q1 | LM62440APPQRJRRQ1 | LM62440APP-Q1 | Pin Selectable | Pin Selectable | Adjustable | 2.1 MHz |
LM62440BPPQRJRRQ1 | LM62440BPP-Q1 | Pin Selectable | Pin Selectable | 3.3 V | 2.1 MHz | |
LM62440CPPQRJRRQ1 | LM62440CPP-Q1 | Pin Selectable | Pin Selectable | 5 V | 2.1 MHz |
In the case where FPWM mode is desired, the conversion from LM61440AFS-Q1 to LM62440APP-Q1 will require a layout change. This is because the change from the LM614xx to the LM624xx requires the resistor (RT resistor for LM614xx and MODE resistor for LM624xx) on Pin 6 to be connected to VIN or an external high voltage for the FPWM mode feature. To have a future-proof PCB layout that enables easy interchange between LM614xx to LM624xx, a top RT resistor between Pin 6 to VIN can be left DNP on the board.
If the FPWM variant of the LM614xx is used then that top RT resistor will be DNP. Alternatively if the LM624xx is used and FPWM mode is required then the bottom MODE resistor to GND is left DNP and the top MODE resistor to VIN is populated. For the case of Auto mode, the Auto mode variant of the LM614xx is used and the bottom RT resistor is populated to set the output voltage. Alternatively if the LM624xx is used and Auto mode is required then the top MODE resistor is left DNP and the bottom MODE resistor is populated.