SNVAA63 March 2023 TPSM365R6
In the standard configuration, the TPSM365R6 IC can tolerate a 65 V difference between its VIN and IC GND pins. In an IBB, however, TPSM365R6 IC GND is referenced to the negative output voltage pin, –VOUT, see Figure 1-1. The TPSM365R6 will experience a potential difference of VIN to –VOUT between its VIN and TPSM365R6 IC GND pins, which effectively limits the input voltage range of the TPSM365R6 module in its inverting buck-boost configuration. For example, for an output voltage of –12 V, the maximum input voltage will be 53 V, as this results in a 65 V potential difference between the TPSM365R6 IC's VIN and GND pins. The output voltage range in the TPSM365R6 IBB topology is –1.8 V to –13 V.