The precise reverse current limit of
the device enables the LM5177 to charge a storage element on the input of the power
stage. Once the integrated average current limitation circuit of the LM5177 is
enabled on the input, the third regulation loop maintains a constant current
operation to charge the storage on the input for example a battery or
super-capacitor array. The end of charge voltage for the input can be regulated by a
simple hysteric regulation approach or by using a linear approach with an external
operational amplifier as well as an equivalent digital regulation scheme.
Once the system power supply is
interrupted or has a malfunction the LM5177 imitatively supplies the connected
system load as soon the selected backup voltage threshold triggers. The seamless
transition is maintained by the buck-boost voltage control loop, which stays in
regulation during charging and ensures a minimum voltage drop for the connected
system during backup.
Benefits:
- Seamless and automatic
transition from main system supply to the power backup
- Combination of energy storage
charging control and backup regulator with a single chip solution
- Single inductor solution,
that is one power stage for charging and backup operation
- Constant current constant
voltage operation possible to realize with
- Adjustable on-the-fly
transition voltage using the output feedback divider
- Scalable solution for
multiple systems. Power levels are adjusted with the BOM. Topologies and
architecture qualification maintains the same.
Below you find a overview for the
control loop interacting together in the DC/DC Backup application. The central point
for the interaction is the COMP pin which defines the peak current target for the
underlying bi-directional peak current control loop
- Internal peak current loop.
The control input signal from the COMP pin sets the bi-directional (positive
and negative pack current) for the PWM logic.
- The internal output voltage
loop is controlling the Vo or system voltage once the system
supply voltage is not there anymore and Vo drops below the
selected voltage by the FB-PIN
- The internal constant current
loop limits and regulates the peak current in the selected direction. For
most power backup cases the negative (charging) current is selected. By
activating the constant current limit the peak current gets clamped and
cannot reach his full value which enables a lower charging current that the
forward discharging current as the forward direction don’t get limited if
the negative direction of the constant current loop is selected.
- The input voltage
(VBAT) constant voltage regulation can be added externally
with a linear regulator in the COMP-pin. Once the battery voltage reaches
the desired target voltage the regulator pulls up the peak current set-point
and the charging operation stops.