SNVSC77 December 2024 LM5125-Q1
ADVANCE INFORMATION
The open-loop response of a boost regulator is defined as the product of modulator transfer function and feedback transfer function. When plotted on a dB scale, the open loop gain is shown as the sum of modulator gain and feedback gain. The modulator transfer function of a current mode boost regulator including a power stage transfer function with an embedded current loop can be simplified as one pole, one zero, and one right-half-plane zero (RHPZ) system.
Modulator transfer function is defined as follows:
where
If the equivalent series resistance (ESR) of Cout (RESR) is small enough and the RHPZ frequency is far away from the target crossover frequency, the modulator transfer function can be further simplified to a one pole system and the voltage loop can be closed with only two loop compensation components, RCOMP and CCOMP, leaving a single pole response at the crossover frequency. A single pole response at the crossover frequency yields a very stable loop with 90 degrees of phase margin.
As shown in Figure 7-1, a gm amplifier is utilized as the output voltage error amplifier. The feedback transfer function includes the feedback resistor divider gain and loop compensation of the error amplifier. RCOMP, CCOMP, and CHF configure the error amplifier gain and phase characteristics, create a pole at origin, a low frequency zero and a high frequency pole.
Feedback transfer function is defined as follows:
where
The pole at the origin minimizes the output steady state error. Place the low frequency zero to cancel the load pole of the modulator. The high frequency pole can be used to cancel the zero created by the output capacitor ESR or to decrease noise susceptibility of the error amplifier. By placing the low frequency zero an order of magnitude less than the crossover frequency, the maximum amount of phase boost can be achieved at the crossover frequency. Place the high frequency pole beyond the crossover frequency because the addition of CHF adds a pole in the feedback transfer function.
The crossover frequency (open loop bandwidth) is usually limited to one fifth of the RHPZ frequency.
For higher crossover frequency, RCOMP can be increased, while proportionally decreasing CCOMP. Conversely, decreasing RCOMP while proportionally increasing CCOMP, results in lower bandwidth while keeping the same zero frequency in the feedback transfer function.