SNVSCE8 July 2024 LM5190-Q1
ADVANCE INFORMATION
The LM5190-Q1 operates with peak current-mode control such that the compensation voltage is proportional to the peak inductor current. During no-load or light-load conditions, the output capacitor discharges very slowly. As a result, the compensation voltage does not demand the driver output pulses on a cycle-by-cycle basis. When the LM5190-Q1 controller detects 16 missed switching cycles, the controller enters sleep mode and switches to a low IQ state to reduce the current drawn from the input. For the LM5190-Q1 to go into sleep mode, the controller must be programmed for diode emulation (tie FPWM/SYNC to AGND).
The typical controller IQ in sleep mode is 15μA with a 12V output.