Please read the LM5171 data sheet (SNVSCM3) and
this user guide before using the EVM. A typical EVM test bench setup is shown in Figure 2-8. The power supplies and loads need to be capable of handling the input and output voltage
and current rating of the board.
By default, onboard 10-V bias supply is
used. External 10-V bias supply can also be applied following the jumper settings described
in Table 2-2
Four external control signals can be used to
operate the EVM, which are UVLO, DIR, EN1/2, and ISETA or ISETD (refer to Figure 2-3).
- UVLO: The main enable command. Apply a
voltage > 2.5 V and < 6 V between J17-pins 5 and 6 to enable the EVM. Pulling the
voltage at J17-pin 5 low keeps the EVM in shutdown mode.
- DIR: the current direction command.
Apply a voltage > 2 V at J17-pin 9 or J18-pin 9 to operate the EVM in Buck Mode.
Apply a voltage < 1 V at the same pin to operate the EVM in Boost Mode. DIR command
can also be programmed using J28. Note that DIR must be either active high or low to
operate the EVM. If the DIR signal is floating, the EVM can not run.
- EN1/2: The channel switching enable
commands. Apply a voltage > 2 V at J17-pin 7 turns on CH-1 converter, and at J17-pin
21 can turn on CH-2 converter. Removing the voltage at the EN1 and EN2 pins to disable
each channel. The channel enable can also be controlled by J29, J30 and J24.
- ISETA or ISETD: The channel current
regulation setting. Applying an analog voltage across J17-pins 11 and 12, or J18-pins 11
and 12, or a PWM signal across J17-pins 13 and 14, or J18-pins 13 and 14, to the EVM
regulates the channel DC current, which is also the power inductor dc current, to a
level proportional the ISETA voltage or ISETD PWM duty ratio. ISETA is set by the
onboard outer voltage loop when closed. Note that, ISETA has 1 V offset, and ISETA=2.2 V
commands the EVM to produce 60 A into or out of the 12VDC-port, depending on the
operation mode.