SNVU894 December 2024 LM5169
The LM5169FEVM has component pads available to make the device compatible with the LM5017 for evaluation compared to the LM5169. Configuring the EVM for the LM5017 requires the following changes:
While the EVM is compatible with the LM5017 using the above changes, the PCB design is optimized for the LM5169. Refer to the LM5017 data sheet for the relevant external component selection criteria.