SPRACN0F October 2021 – March 2023 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Starting in 1997, Texas Instruments integrated flash memory, an Analog-to-Digital Converter (ADC), a Digital Signal Processor (DSP) , and Pulse Width Modulation (PWM) units on a single device. The first C2000 real-time control MCU was born.
Over more than two decades, this device family grew and now millions of C2000's can be found in numerous applications in industrial and automotive applications like Motor Control, Solar Inverters, Digital Power, Electrical Vehicles and more (see #GUID-A8BC3D2C-5F37-47C8-B571-415A50A586A0). There is one tie that binds all the above applications; their real-time nature and the need for a real-time controller.
A real-time control system is typically composed of four main elements: see #T5843526-2:
The key to real-time control is to minimize the time between Sensing, Processing and Control: this time is defined as the Real-Time Signal Chain. #GUID-83981EAD-BC90-4152-A06F-A8E411260568 illustrates how the entire process is critical to understand the overall system performance of a real-time controller, vs simply looking at the time it takes the main processing unit to complete the control algorithm (step 4).
Many benchmarks, only focus on the time is takes to complete the step 4, typically expressed in Millions Instructions Per Second (MIPS) while the real-time challenge for designers is to minimize the time between Sample to Output: the real-time MCU architecture choice is critical.
The C2000 real-time MCU is a scalable, ultra-low latency, real-time controller platform designed for efficiency in power electronics, such as high power density, high switching frequencies, GaN and SiC technologies and was designed with the best Real-Time Signal Chain performance in mind and can deliver 2-times more real-time signal chain performance than an Arm®-based architecture.
The following sections showcase these advantages in terms of CPU cycle counts for easy comparison:
The next sections will zoom in each key elements that enables C2000 MCUs to deliver the best real-time signal performance in the market. Backed up with 25 years of expertise, which has translated in the largest reference design offering for power conversion in the industry, coming with robust production ready software and open source hardware documentation, designers can now innovate to and build energy system of the future. The C2000 real-time MCU continues to expand with a platform of software compatible device from the low-end to the high-end. Check the home page on TI.com and register for the TI newsletter to stay up to date on new innovations from C2000 real-time MCUs.