SPRACN0F October 2021 – March 2023 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
A sigma-delta type ADC is by design an over-sampling architecture. The ADC itself is a single bit design that over-samples the signal of interest to produce a higher order output. The modulation of this type of converter results in a binary output and, hence, a serial data stream. This serial data stream is then sent to the filter/demodulator on the C2000 MCU for re-construction into a higher bit order digital representation of the sampled signal (#T5843526-183) .
At this point an interrupt is generated to the MCU, informing the other domains there is new data to process and act upon.
The SDFM module on the C2000 MCU is unique in that not only can the converted data be read post filtering, but the PWMs can be switched based on this data automatically. Each SDFM module contains four channels. Inside each channel exists two filters: a primary filter that produces the SDFM data and a secondary filter containing both high and low limit comparators (#T5843526-182). This allows the system to control the PWM signals without waiting for CPU intervention, resulting in both lower latency as well as lower overall CPU utilization.