SPRACO3 October 2019 INA240 , LMG5200 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
There are two GUIs available to perform the frequency response analysis: one (SFRA_GUI) to plot open loop and plant Bode diagram, and another (SFRA_GUI_MC) to plot open loop and closed loop Bode diagram. They can be invoked and connected to the target platform to study the control loops. The GUI executables are available in the location as mentioned in Section 7.6.1.
This demo uses the GUI 'SFRA_GUI_MC'. However, it is encouraged to experiment with the SFRA_GUI as well to study the plant. With the SFRA_GUI, you can plot the same graph as in SFRA_GUI_MC by passing the argument 'SFRA_GUI_PLOT_GH_CL' in the function configureSFRA() as shown in the code snippet below:
configureSFRA(SFRA_GUI_PLOT_GH_H, M1_SAMPLING_FREQ);
But the inferences from the plots are not according to that in SFRA_GUI_MC. Therefore, it is advised to configure SFRA for 'SFRA_GUI_PLOT_GH_H' so that you can see open loop, closed loop and plant model plots using these two GUIs, by using one at a time.