SPRACP4A December 2019 – June 2024 AM67 , AM67A , AM68 , AM68A , AM69 , AM69A , DRA821U , DRA821U-Q1 , DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VM-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
Match the etch lengths of the relevant differential pair traces. Intra-pair skew is the term used to define the difference between the etch length of the + and – lane of a differential pair. Inter-pair skew is used to describe the difference between the etch lengths of a differential pair from another differential pair of the same group. The etch length of the differential pair groups do not need to match. For example the etch lengths of USB 3.0 TX and RX do not need to match. There are also standards that do not have a Interpair skew requirement because the different lanes do not have to be the same length. When matching the intra-pair skew of the high-speed signals, add serpentine routing to match the lengths as close to the mismatched ends as possible, see Figure 2-1.