SPRACP4A December 2019 – June 2024 AM67 , AM67A , AM68 , AM69 , DRA829J , DRA829V , TDA4AEN-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VM , TDA4VM-Q1
The PCIe interface on the device is compliant with the PCIe revision 3.0 specification. Refer to the PCIe specifications for all the described connections. Those recommendations are more descriptive and exhaustive than what is possible in this application note. The PCIe Motherboard Checklist 1.0 document is also available from PCI-SIG (www.pcisig.com).
The following sections contain suggestions for any PCIe connection that is not described in the official PCIe specification, such as an onboard Device-to-Device or Device-to-other PCIe compliant processor connection.
The use of PCIe compatible bridges and switches is allowed for interfacing with more than one other processor or PCIe device.