SPRACS8 May 2022 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
Function name: I2C_MasterTransmitter(I2CA_BASE, struct I2CHandle *pI2C_Params)
Description: This function can be used to transmit 'N' number of bytes defined in pI2C_Params. This function can be used to perform following EEPROM write operations.
Set EEPROM.NumOfDataBytes = 1, because one byte needs to be transmitted
Set EEPROM.NumOfDataBytes = 2, because two bytes needs to be transmitted
Set EEPROM.NumOfDataBytes = 'N', because 'N' bytes needs to be transmitted - Page size depends upon EEPROM chosen
Below setting applies to all the above EEPROM write operations
Set EEPROM.NumOfAddrBytes = 2, because high address byte and low address byte needs to be transmitted
Arguments:
base : base is the base address of the I2C instance used
pI2C_Params : Pointer to I2C address handle of the slave
Return:Status of I2C transaction