Additional details of each parameter
of this section can be found in the list below:
- VREF Control:
- VREF Range (DQ or
CA): This parameter corresponds to MR14[6] for DQ signals and
MR12[6] for command / address signals, and defines which VREF range is
used for the respective signals.
- VREF (DQ or CA):
This parameter corresponds to MR14[5:0] for DQ signals and MR12[5:0] for
command / address signals, and defines the target reference voltage
level, as a percentage of the I/O voltage.
- Drive Strength:
- Pull-Down (PDDS):
This parameter corresponds to MR3[5:3] of the LPDDR4 memory and defines
the drive strength of the DDR data (DQ) and strobe (DQS) pins during
READ cycles. As discussed in Section 2.3.1, the appropriate value should be selected based on the I/O model
settings used to achieve the best simulation results.
- Pull Up
Calibration: This parameter corresponds to MR3[0] of the LPDDR4
memory and defines the target VOH during READ cycles. It is recommended
to leave this parameter set to the default, "VDDQ / 3".
- Termination:
- CA ODT Disable:
This parameter corresponds to MR22[5] of the LPDDR4 memory. When this
parameter is set to "Disable", the termination of the command / address
pins are disabled regardless of how the termination is configured in
MR11 or the state of the ODT_CA pin. When this parameter is set to
"ODT_CA Bond Pad", the termination of the command / address pins are
configured based on the MR11 configuration along with the ODT_CA pin. It
is recommended to leave this parameter set to the default, "ODT_CA Bond
Pad".
- CK ODT Override:
This parameter corresponds to MR22[3] of the LPDDR4 memory. When set to
"Enable", the clock termination is determined by the MR11 configuration
regardless of the ODT_CA pin. This parameter is used to enable
termination on the clock when the CA bus is shared between two ranks,
but the clock is not. Because the Jacinto 7 processors share both the CA
bus and clock between ranks, it is recommended to leave this parameter
set to the default, "Disable".
- CS ODT Override:
This parameter corresponds to MR22[4] of the LPDDR4 memory. When set to
"Enable", the chip select termination is determined by the MR11
configuration regardless of the ODT_CA pin. This parameter is used to
enable termination on the chip select pin when the CA bus is shared
between two ranks, but the chip select is not. Because the Jacinto 7
processors share the CA bus between ranks but have unique chip select
signals, it is recommended to leave this parameter set to the default,
"Enable".
- CA ODT: This
parameter corresponds to MR11[6:4] of the LPDDR4 memory and defines the
termination of the command / address pins of the LPDDR4 memory. As
discussed in Section 2.3.1, the appropriate value should be selected based on the I/O model
settings used to achieve the best simulation results.
- DQ ODT: This
parameter corresponds to MR11[2:0] of the LPDDR4 memory and defines the
termination of the data (DQ), data mask (DM), and strobe (DQS) pins of
the LPDDR4 memory during WRITE cycles. As discussed in Section 2.3.1, the appropriate value should be selected based on the I/O model
settings used to achieve the best simulation results.
- SOC ODT: This
parameter corresponds to MR22[2:0] of the LPDDR4 memory and defines the
termination of the processor / DDR controller. This parameter must be
configured to match the termination as defined in 3.