SPRACZ9A November 2021 – December 2022 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
A buildup of electrical charge can result in electrostatic discharge (ESD) to the device while in operation. Care should be taken when handling these microcontrollers and when storing them. All of the F2800x devices are tested to comply with the TI standard ESD specifications, including the peripherals and the port pins. They are rated to withstand the following ESD tests: human-body model (HBM), at 2 kV and charged-device model (CDM) at 500 V.
A supply voltage glitch or ESD will put the device in an unknown state. Therefore, it is important to have a good PCB layout for optimum noise and ESD performance. The similar ESD protection diodes can be utilized for JTAG pins as well. Keep the loop area of critical traces (in this case, JTAG, XRS, X1, X2) as small as possible. If your design needs to bring any pin, like a GPIO, to a connector (for external connectivity) be sure to take special ESD care by adding ESD protection parts. Some systems may require mechanical fixes like metallic shielding, rerouting of cabling, and so forth, to maintain ESD protection. When using these external ESD protection devices, be sure to carefully follow the layout guidelines specified in the device-specific data sheet to maximize its effectiveness.