SPRACZ9A November 2021 – December 2022 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
The ADCs onboard use VREFHIx and VREFLOx as voltage references. For most applications, the internal voltage references offer sufficient performance. The VREFHIx pin voltage is thus driven by an internal bandgap voltage reference whose voltage can be selected as a 1.65 V output (0 V to 3.3 V) or a 2.5 V output (0 V to 2.5 V). If even more accuracy is a design requirement for the system being implemented, then an external reference voltage can be used instead.
When using the internal reference mode, no additional voltage sources should be placed on the VREFHI pin as the voltage is driven onto this pin by the device itself. In external reference mode, externally drive the high reference voltage pin using an external circuit, such as REF3030 and high-speed operational amplifier. This voltage must be 2.4 V to VDDA. In all instances, ensure a 2.2 µF capacitor is placed on the pin.