This application note is to describe how to make the DDR system implementation of AM62x, AM62Lx processor board designs straightforward for all designers. The requirements have been distilled down to a set of layout and routing rules that allow designers to successfully implement a robust design for the topologies TI supports. The topics in this document include the board layout guidelines, board stackup, supported implementations, schematics, component placement, and trace length matching targets.
All trademarks are the property of their respective owners.
The AM62x, AM62Lx processors support two different types of DDR memories: DDR4 and LPDDR4. This allows customer board designs to be implemented with the memory type that best meets the target market at the lowest possible DDR SDRAM cost. This document has generic information that is applicable to both DDR4 and LPDDR4, as well as separate sections that are specific to each supported DDR memory type.