SPRAD21E May 2023 – February 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1
For naming the peripherals and instances, the device-specific TRM tends to be generic and the device-specific data sheet is specific.
In the data sheet a suffix number is assigned even when there is only one peripheral instance, so any documents that reference the peripheral name will not need to change from processor to processor.
The suffix starts with “0”. For the CPSW3G port names, port “0” is the internal (CPPI host) port of the switch.