General
Review and verify the following for
the custom schematic design:
- Add provision to isolate the
IOs that can be used for debug from alternate function
- Add provision for connecting
UART interfaces for debug during initial board build
- Add provision for JTAG
connector or Test points for JTAG interface connection including ESD diodes.
Please the pulls as per pin connectivity requirements near to the processor
JTAG interface pins
Schematic Review
Follow the below list for the custom
schematic design:
- The required pullup and
series resistors are provided for the UART interfaces used for debug when
external interface signals are directly connected to the processor UART
signals
- External ESD protection when
external interface signals are directly connected to the processor UART
signals
Additional
- Processor UART and most of the IO
signals are not fail-safe. Recommendation is to apply external inputs only after
the processor supplies ramp
- The recommendation is to
disconnect the external interface signals when processor board is powered
off
Refer [FAQ] SK-AM62: Purpose Of Different
UARTs.