SPRAD51A December 2023 – April 2024 TMS320F2800157 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28P659DK-Q1
Flash kernel source and project files for Code Composer Studio (CCS) are provided in C2000Ware, in the corresponding device’s examples directory. Load the project into CCS and build the project. These projects have a post-build step in which the compiled and linked .out file is converted into the correct boot hex format needed by either the CAN or MCAN ROM bootloader and is saved as the example name with a .txt extension.