SPRAD51A December 2023 – April 2024 TMS320F2800157 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28P659DK-Q1
The hardware components needed to run the examples are a C2000 device connected to a CAN transceiver, and a PEAK PCAN-USB Pro FD Analyzer. For controlCards, a custom-designed CAN transceiver board needs to be used, as well as the HSEC-180-pin ControlCard Docking Station. The custom-designed transceiver board is connected to the ControlCard using four connections: ground, 3.3V, CANTX and CANRX.
The LaunchPad™ devices contain an on-board CAN transceiver. The PEAK PCAN-USB Pro FD Analyzer is connected to the LaunchPad through the ground, CAN-Lo and CAN-Hi connections. The onboard CAN Routing switch needs to be set low for the transceiver to communicate using the GPIOs.
After building the kernels in CCS, it is important to setup the device correctly to be able to communicate with the host PC running the host programmer. The first thing to do is make sure the boot mode value is configured correctly to boot the device to CAN/MCAN Boot mode. Next, connect the MCAN TX and RX pins using a transceiver to the CAN port on the host side.