SPRAD55A March   2023  – August 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28P650DK

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Theory
  6. 3Software Oversampling
  7. 4Hardware Oversampling
  8. 5Results
  9. 6Summary
  10. 7References
  11. 8Revision History

Summary

This application note covered the effects of oversampling with an ADC using software and hardware methods, and how oversampling can increase the effective number of bits (ENOB). The theoretical ENOB increases by 0.5 every time the oversampling factor is doubled. The observed ENOB increase is slightly lower due to system noise limitations. This can be further improved by adding a buffer to the ADC input and using an external VREF source. Oversampling does decrease the rate at which individual samples are read, since the oversampling takes up additional time within the control loop. There is also an increase in time to collect results from the ADC, depending on the oversampling factor.