SPRADE8A November 2023 – April 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The EEPROM_Get_64_Bit_Data_Address is largely unchanged in the Single-Unit implementation, but the behavior upon detecting a full EEPROM unit is different.
if(Bank_Pointer > End_Address-3) // Test if EEPROM is full
{
Erase_Inactive_Unit = 1;
Erase_Blank_Check = 1;
EEPROM_Erase();
Erase_Inactive_Unit = 0;
RESET_BANK_POINTER;
}
As shown above, if the EEPROM unit is full, it is simply erased, performs a blank check and the pointer is reset to the beginning of the unit.