SPRADE8A November 2023 – April 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
If using the Ping Pong method, the following diagram shows the implemented behavior. As shown in Figure 3-2, there are two EEPROM units made up of selected Flash Sectors. One is marked as an Active Unit, and the other is marked as the Inactive Unit. To begin, data is written to the Active Unit.
If the Active Unit is full and there is more data to be written, the Active and Inactive EEPROM units will switch. Therefore, the previously Active Unit (full Unit) will be marked as Inactive, and the previously Inactive Unit (empty Unit) will be marked as Active. Subsequently, the data will be written to the newly Active EEPROM Unit. After the data is successfully programmed to the Active EEPROM Unit, the Inactive EEPROM Unit is erased. This method ensures that there is a fall-back options for the last successfully written data in case of any failure during the erase or program operation when the currently active EEPROM Unit is full.
This process can be repeated as necessary.