SPRADG1 February 2024 AM625 , AM625-Q1 , AM625SIP
This setup requires an HDMI connection to a monitor.
To simplify the process, this is a simple bash script to infinite run the Jellyfish example.
#!/bin/sh
for i in $(seq 3); do
glmark2-es2-wayland -b jellyfish --run-forever > /dev/null &
done
wait
Then the script needs to be copied onto the SD Card.
HOST$ sudo cp <GPU Script> /media/<USER>/root/home/root
root@am62xx-evm:~# systemctrl stop ti-apps-launcher
root@am62xx-evm:~# systemctrl disable ti-apps-launcher
root@am62xx-evm:~# systemctrl start weston
root@am62xx-evm:~# ./<GPU Script>.sh
To exit the bash script, send an interrupt into the terminal with CTRL + C.