SPRADH0 August 2024 AM625 , AM6442 , AM69 , TDA4VM
There are two methods of activating the license. See this link for more details on these two methods: Licensing of Products (helpme-codesys.com)
Online activation - requires the CODESYS Development System to have internet access, the EtherCAT controller (target system) does not require internet access
Offline activation - requires using CodeMeter Control Center, which is installed with the CODESYS Development System installation
Online activation through the License Manager diaglog on the CODESYS Development System can not be possible if the CODESYS Development System connected to the EtherCAT network with a direct Ethernet connection or through a switch without DHCP router services.
The license must also be activated on a device (EtherCAT controller) or USB dongle. CODESYS calls what the license is activated on as a "container". A device is called "soft container" and the USB dongle is called "Dongle" or "Key".
The key differences between activation on a Soft Container and activation on a Dongle are listed below. The same list can be found at this site CODESYS Key
ACTIVATION METHOD | ADVANTAGES | DISADVANTAGES |
---|---|---|
Software license container (SoftContainer) |
|
|
CODESYS Key (dongle) |
|
|