SPRADJ1A June 2024 – August 2024 TMS320F280021 , TMS320F280023 , TMS320F280023C , TMS320F280025 , TMS320F280025C , TMS320F280033 , TMS320F280034 , TMS320F280037 , TMS320F280037C , TMS320F280039 , TMS320F280039C , TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280049 , TMS320F280049C , TMS320F28075 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK
During the normal operation condition after the soft start, the burst mode control is implemented to reduce the control gain during light load or no-load conditions. Different with the control schemes in the soft start, the deadtime value of PWM only uses two fixed values, normal one and larger one, which is used to disable PWM output. Thus, compared to the control algorithm in Figure 4-2, it removes the duty cycle adjustment mode by setting the deadtime to a maximum value when Vc_v is lower than 0, as shown in Figure 4-3.