SPRADN6 November 2024 F29H850TU , F29H859TU-Q1
Real-time microcontrollers (MCU) play a crucial role in helping high-voltage automotive and energy infrastructure systems meet power efficiency, power density, and safety design requirements. From onboard chargers (OBC) to uninterruptible power supplies (UPS), these devices must deliver fast, deterministic performance for time-critical tasks in harsh environments.
F29H85x series C2000™ MCUs, built with TI's C29 core, are designed to meet demanding processing and safety design challenges in high-voltage systems. These MCUs deliver enhanced performance, two to five times that of the previous TI C28 core and other MCUs on the market, and feature advanced integrated safety and security components – helping engineers optimize system reliability and integrity, while reducing design complexity and cost.
Innovations in the C29 core include:
This article explores how real-time control MCUs like the F29H859TU-Q1 and F29H850TU and their C29 cores help engineers deliver increased processing capabilities, power efficiency, and fast switching frequencies in subsystems for electric vehicles (such as OBC and high- and low-voltage DC/DC converters) and energy infrastructure (such as solar inverters and UPS).
By using a more integrated design approach in electric vehicle subsystems like OBC, high- and low-voltage DC/DC converters, and host integration systems, designers can increase power efficiency, reduce system cost and weight, and streamline management of safety functions in their designs.
Typically, executing multiple applications within a single MCU requires having a dedicated core per function. For example, one core is dedicated to the OBC and another is dedicated to the high- and low-voltage DC/DC converter. Using an F29H85x series MCU, designers can allocate two of the MCU's three cores in lockstep to handle key functions that are required for a host MCU, such as AUTOSAR and crucial safety and security tasks at an ASIL-D integrity level, while the remaining core handles control functions in the system.
The C29 core integrates with the safety and security unit (SSU) to enable seamless execution of multiple control functions in the same core while preventing the functions from interfering with one another. This maintains full isolation and freedom from interference between the functions.
F29H85x series MCUs further enhance performance in automotive systems by enabling the use of new control topologies and algorithms, such as the matrix converter topology, which are enabled through the enhanced EPWM features. These features include a complex compare scheme that also integrates safety checks like guaranteed minimum dead band and illegal combo logic. Additionally, integrated ADCs in these MCUs help enable accurate sensing with features such as hardware oversampling and a results safety checker to minimize the software overhead needed for common tasks.
Similar to challenges for automotive systems, designers of energy infrastructure applications must meet growing demand for higher system efficiency. Systems supporting energy infrastructure, like solar inverters and UPS (Figure 1), must deliver increasing amounts of energy, while also protecting against cyberattacks.
To achieve higher power efficiency and density, designers can leverage wide-bandgap semiconductors (SiC and GaN) and F29H85x series MCUs to increase power electronic switching and control loop frequencies. Increasing control loop frequencies increases system power efficiency and density for power conversion, while allowing for the use of smaller passive components, such as capacitors and inductors, which further reduces board space usage.
From a security perspective, integrating the hardware security module (HSM) and SSU with the C29 core helps protect energy infrastructure from potential malware. The SSU helps prevent malware from interrupting ongoing functions within the MCUs while maintaining protection of memory and peripherals without compromising real-time performance. The SSU automatically manages and switches memory and peripheral access permissions in hardware. The SSU, in conjunction with the C29 CPU, manages independent stack pointers and stack memory for each isolated application function, providing security protection against malware and other cyberattacks.
The F29H85x MCU's architecture supports A/B flash bank which facilitates live firmware updates (LFU) with almost zero downtime. In addition to the basic flash controller verification of contents after programming, the HSM verifies the overall integrity of the update. The architecture also features the ability to rollback software updates to the previous version and can permanently block rollbacks for critical security updates.
As demand for efficient and secure energy designs continues to grow, F29H85x series MCUs and C29 cores are helping drive the future of high-voltage applications. These highly capable MCUs allow designers to expand their current systems by simplifying design, reducing costs, and enhancing reliability.