SPRADP0 December   2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1List of Acronyms
  5. 2Software Setup
  6. 3Hardware Setup
    1. 3.1 AM263x Connections
    2. 3.2 AM263Px Connections
    3. 3.3 Lauterbach® Connections
  7. 4Building MCU_PLUS_SDK Examples
    1. 4.1 CCS Import And Build
    2. 4.2 Command Line Build
  8. 5CMM Scripts
    1. 5.1 AM263x CMM Script
    2. 5.2 AM263Px CMM Script
  9. 6Flashing SBL Null
    1. 6.1 Using UniFlash tool
    2. 6.2 Using Command Line Python Scripts
  10. 7Debugging with Trace32 Software
  11. 8Summary
  12. 9References

AM263x Connections

  1. Dock the AM263x device on the HSEC Dock breakout board.
  2. Connect the power supply to the HSEC Dock breakout board.
  3. Connect the USB Type-A to micro-B from the Host PC to the AM26x microcontroller.
  4. On the AM263Px, put the SW-5 switch to OFF to disconnect the on-board debugger.

    Switch

    State

    SW-5

    Low

  5. Power on the HSEC Dock breakout board. Users now see the LD1, LD6, LD14, LD15 glowing on the AM263x.
 AM263x PCB# PROC E2 SW-5
                    Switch Figure 3-1 AM263x PCB# PROC E2 SW-5 Switch
 AM263x Control Card Mounted on
                    HSEC Dock Board Figure 3-2 AM263x Control Card Mounted on HSEC Dock Board