The device deploys Texas Instrument's CTools debug technology for on-chip debug and trace support. It provides the following features:
- External debug interfaces:
- Primary debug interface - IEEE1149.1 (JTAG)
- Used for debugger connection
- Controls
ICEPick™ (generic test access port [TAP] for dynamic TAP insertion) to allow the debugger to access several debug resources through its secondary (output) JTAG ports (for more information, see Section 33.3.3.1, ICEPick Secondary TAPs).
- For more information about IEEE1149.1, see Section 33.2.1, IEEE1149.1.
- Debug (trace) port
- Can be used to export processor or system trace off-chip (to an external trace receiver)
- Can be used for cross-triggering with an external device
- Configured through debug resources manager (DRM) module instantiated in the debug subsystem
- For more information about debug (trace) port, see Section 33.2.2, Debug (Trace) Port , and Section 33.11, Concurrent Debug Modes.
- JTAG based processor debug on:
- Cortex-A15 (x2) in MPU
- C66x in DSP1, DSP2
- Cortex-M4 (x2) in IPU1, IPU2
- Arm968 (x2) in IVA
- ARP32 in EVE1, EVE2
- Dynamic TAP insertion
- Controlled by ICEPick
- For more information, see Section 33.3.3, Dynamic TAP Insertion.
- Power and clock management
- Debugger can get the status of the power domain associated to each TAP.
- Debugger may prevent the application software switching off the power domain.
- Application power management behavior can be preserved during debug across power transitions.
- For more information, see Section 33.6.1, Power and Clock Management.
- Reset management
- Debugger can configure ICEPick to assert, block, or extend the reset of a given subsystem.
- For more information, see Section 33.6.2, Reset Management.
- Cross-triggering
- Provides a way to propagate debug (trigger) events from one processor, subsystem, or module to another:
- Subsystem A can be programmed to generate a debug event, which can then be exported as a global trigger across the device.
- Subsystem B can be programmed to be sensitive to the trigger line input and to generate an action on trigger detection.
- Two global trigger lines are implemented
- Device-level cross-triggering is handled by the XTRIG (TI cross-trigger) module implemented in the debug subsystem
- Various Arm® CoreSight™ cross-trigger modules implemented to provide support for CoreSight triggers distribution
- CoreSight Cross-Trigger Interface (CS_CTI) modules
- CoreSight Cross-Trigger Matrix (CS_CTM) modules
- For more information about cross-triggering, see Section 33.4.2, Cross-Triggering.
- Suspend
- Provides a way to stop a closely coupled hardware process running on a peripheral module when the host processor enters debug state
- For more information about suspend, see Section 33.4.3, Suspend.
- MPU watchpoint
- Embedded in MPU subsystem
- Provides visibility on MPU to EMIF direct paths
- For more information, see Section 33.8, MPU Memory Adaptor (MPU_MA) Watchpoint
- Processor trace
- Cortex-A15 (MPU) and C66x (DSP) processor trace is supported
- Program trace only for MPU (no data trace)
- MPU trace supported by a CoreSight Program Trace Macrocell (CS_PTM) module (per MPU core)
- Three exclusive trace sinks:
- CoreSight Trace Port Interface Unit (CS_TPIU) – trace export to an external trace receiver
- CTools Trace Buffer Router (CT_TBR) in system bridge mode – trace export through USB
- CT_TBR in buffer mode – trace history store into on-chip trace buffer
- For more information, see Section 33.9, Processor Trace.
- System instrumentation (trace)
- Supported by a CTools System Trace Module (CT_STM), implementing MIPI System Trace Protocol (STP) (rev 2.0)
- Real-time software trace
- MPU software instrumentation through CoreSight STM (CS_STM) (STP2.0)
- System-on-chip (SoC) software instrumentation through CT_STM (STP2.0)
- OCP watchpoint (OCP_WP_NOC)
- OCP target traffic monitoring: OCP_WP_NOC can be configured to generate a trigger upon watchpoint match (that is, when target transaction attributes match the user-defined attributes).
- SoC events trace
- DMA transfer profiling
- Statistics collector (performance probes)
- Computes traffic statistics within a user-defined window and periodically reports to the user through the CT_STM interface
- Embedded in the L3_MAIN interconnect
- 10 instances:
- 1 instance dedicated to target (SDRAM) load monitoring
- 9 instances dedicated to master latency monitoring
- IVA instrumentation (hardware accelerator [HWA] profiling)
- Supported through a software message and system trace event (SMSET) module embedded in the IVA subsystem
- EVE instrumentation (hardware accelerator [HWA] profiling)
- Supported through a software message and system trace event (SMSET) module embedded in the EVE subsystem
- Power-management events profiling (PM instrumentation [PMI])
- Monitoring major power-management events. The PM state changes are handled as generic events and encapsulated in STP messages.
- Clock-management events profiling (CM instrumentation [CMI]) for CM_CORE_AON clocks
- Monitoring major clock management events. The CM state changes are handled as generic events and encapsulated in STP messages.
- For more information, see Section 33.10, System Instrumentation.
- Performance monitoring
- Supported by subsystem counter timer module (SCTM) for IPU
- Supported by performance monitoring unit (PMU) for MPU subsystem
- For more information, see Section 33.7, Performance Monitoring.