SPRUIY3 February 2023 TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
Some GPIOs on this device are multiplexed with analog pins. These are also referred to as AGPIOs. Unlike AIOs, AGPIOs have full input and output capability.
By default the AGPIOs are not connected and have to be configured. Table 3-9 shows how to configure the AGPIOs.
AGPIOCTRLA.GPIOy (Default = 0) |
GPAxMSEL.GPIOy (Default = 1) |
Pin Connected To: | |
---|---|---|---|
ADC | GPIOy | ||
0 | 0 | - | Yes |
0 | 1 | -(1) | -(1) |
1 | 0 | - | Yes |
1 | 1 | Yes | - |