Select instances of the
(full) CMPSS module can optionally route the low DAC output to an external
pin to be used as an external DAC. This is subject to the following
constraints:
- This is available
only on select instances; consult the device data sheet to
determine if the CMPSS DAC has been pinned out for a
particular instance.
- This functionality is never available on CMPSS_LITE
modules.
- All other CMPSS
module functionality is unusable when the output DAC is
enabled. This includes the high DAC, both comparators, ramp
generation logic, and the digital filters.
- See the device
data sheet for effective resolution of the CMPSS DAC
output.
Note: The
CMPSS low DAC output does not necessarily appear on the same pins
that are available for low comparator input. Consult the pinout of
the device data sheet to determine which pin the CMPSS output DAC is
available on.