SPRUJ42E March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
PRODUCTION DATA
Enet Port N Tx Egress InterVLAN D
Return to Summary Table
Offset = Base + (k * 1000h); where k = 0 to 1d
Instance Name | Physical Address |
---|---|
CPSW0 | 5282 23BCh + formula |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
NONE | |||||||
0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
NONE | |||||||
0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DECREMENT_TTL | DEST_FORCE_UNTAGGED_EGRESS | REPLACE_DA_SA | REPLACE_VID | VID | |||
R/W | R/W | R/W | R/W | R/W | |||
0h | 0h | 0h | 0h | 0h | |||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
VID | |||||||
R/W | |||||||
0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31:16 | RESERVED | NONE | 0h | Reserved |
15 | DECREMENT_TTL | R/W | 0h | Decrement Time To Live - When set, the Time To Live (TTL) field in the header is decremented. IPV4 - Decrement the TTL byte and update the Header Checksum. IPV6 - Decrement the Hop Limit. note: When this bit is set, the ALE should be configured to send any IPv4/6 packet with a zero or one TTL field to the host with the ALE egress operation ttl_check bit.When this bit is cleared the TTL/Hop Limit fields are not checked or modified. |
14 | DEST_FORCE_UNTAGGED_EGRESS | R/W | 0h | Destination VLAN Force Untagged Egress - When set, this bit indicates that the VLAN should be removed on egress for the routed packet. The replace_vid bit should be set for this bit to be used, otherwise force untagged egress comes from the address lookup engine. |
13 | REPLACE_DA_SA | R/W | 0h | Replace Destination Address and Source Address - When set this bit indicates that the routed packet destination address should be replaced by da[47:0] and the source address should be replaced by sa[47:0]. |
12 | REPLACE_VID | R/W | 0h | Replace VLAN ID - When set this bit indicates that the VLAN ID should be replaced for the routed packet. |
11:0 | VID | R/W | 0h | VLAN ID |