SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
FILE: fsi_ex2_periodic_frame.c
Example sets up infinite data frame transfers where trigger comes from ISR handling the periodic CPU Timer event. Automatic(Hw triggered) Ping frame transmission is also setup along with data.
CPU Timer0 is chosen for setting up periodic timer events. User can choose any other Timer-1/Timer-2 as well.
Automatic(Hw triggered) Ping frame transmission is also setup along with data.
If there are any comparison failures during transfers or any of error event occurs, execution will stop.
External Connections