SPRUJ79 November 2024 F29H850TU
This section details the aspects of the ESC integration in the MCU. On this MCU, the ESC is integrated such that the ESC is accessed by either the CPU1 (main) subsystem or the CPU2 or the CPU3 subsystem. The MCU with the ESC functions as an EtherCAT SubordinateDevice device.
Figure 35-7 shows the ESC on this MCU.
ESC Figure Sections | More Information Links |
---|---|
ECAT/ESCSS Clocking | ESC Clocking |
Resets | ESCSS Resets |
Service Request | SYNC Signals Interrupts and Interrupt Mapping |
Registers and PDI | ESC SubSystem |
Distributed Clocks | Distributed Clocks - Sync and Latch |
LEDS and Link | LED Controls |
Inputs Outputs | General Purpose Inputs and Outputs |
Physical Layer | EtherCAT Physical Layer |
EEPROM | SubordinateDevice Node Configuration and EEPROM |
There are various actions that the controlling processor (CPU1/CPU2/CPU3) needs to perform in response to actions initiated by the EtherCAT MainDevice meant for this particular SubordinateDevice . All these interactions take place through one of the following: