SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
The MCAN module generates interrupt requests and is configured using the Host CPU. The Suspend mode prevents the interrupt requests from propagating to the Host CPU. The MCAN core has two interrupt lines and 30 internal interrupt sources. Each source can be configured to drive one of the two interrupt lines. The interrupts are level high interrupts. The MCAN core provides two interrupt requests (MCANSS_INT0 and MCANSS_INT1).
For more information, see the following registers:
The MCAN module supports External Timestamp Counter. The External Timestamp Counter produces an interrupt when the count rolls over (see Section 34.5.10.1).
For more information, see the following registers:
To clear IRQ_INT0, IRQ_INT1, and TS_WAKE interrupts, write to the EOI bit field for the corresponding interrupt number that is described in the MCANSS_EOI register. When the MCAN is used by the CPU, in addition to clearing the interrupt sources, additional operations are warranted in the PIPE module (refer to the Configuring Interrupts section of the Peripheral Interrupts Priority and expansion chapter) for successive MCAN interrupts to be recognized.
The MCAN module is capable of issuing an ECC interrupt. After clearing the ECC interrupt source, the application software must also write a 1 to the EOI registers (MCANERR_SEC_EOI.EOI_WR/ MCANERR_DED_EOI.EOI_WR). For more information, see Section 34.5.12.2.