SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
Improvements from the Type 0 HRCAP are:
The HRCAP enhancement has been added to eCAP 5 and eCAP 6 to allow signals to be captured asynchronously to SYSCLK. Each HRCAP submodule includes one capture channel in addition to a hardware calibration block. All eCAP hardware is accessible when using the HRCAP enhancements; however, using the Event Filter or the Input Qualifier is not valid, as these are synchronous to SYSCLK.
Each HRCAP-capable channel has the following independent key resources: