SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
On Type 0 eCAP modules, the CPU was required to begin data transfers using RTDMA. New to the Type 1 eCAP, a separate RTDMA Trigger (ECAP_DMA_INT) enables continuous transfer of capture data from eCAP registers to on-chip memory using RTDMA. Any one of the four available interrupt events (LD1, LD2, LD3, and LD4) can be selected as the trigger source for ECAP_DMA_INT using ECCTL2 [DMAEVTSEL].
New to the Type 3 eCAP is the ability to trigger RTDMA events in APWM mode. Any one of three available events (period match, compare match, or both) can be selected as the trigger source for ECAP_DMA_INT using ECCTL2 [DMAEVTSEL].