SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
ECAP supports accurate time capture of events that can be relatively checked against the series of events in vicinity and used for the control loop action. Additionally, ECAP has inbuilt capability of limited PWM action that can be triggered based on the selected input. Hence, the SYNC0/1 are also connected to ECAP input mux. The exact select value/vector for SYNC0/1 is defined in the Enhanced Capture (eCAP) chapter.