Returns information about this compile
of the Flash API.
Synopsis
Fapi_LibraryInfoType Fapi_getLibraryInfo(void)
Description
This function returns information
specific to the compile of the Flash API library. The information is returned in a
struct Fapi_LibraryInfoType. The members are as follows:
- u8ApiMajorVersion – Major version
number of this compile of the API. This value is 2.
- u8ApiMinorVersion – Minor version
number of this compile of the API. Minor version is 0 for F280013x/F280015x
devices.
- u8ApiRevision – Revision version
number of this compile of the API.
Revision number is 10 for this
release.
- oApiProductionStatus – Production
status of this compile (Alpha_Internal, Alpha, Beta_Internal, Beta,
Production).
Production
status is Production for this release.
- u32ApiBuildNumber – Build number
of this compile.
- u8ApiTechnologyType – Indicates
the Flash technology supported by the API. This field returns a value of
0x5.
- u8ApiTechnologyRevision –
Indicates the revision of the technology supported by the API
- u8ApiEndianness – This field
always returns as 1 (Little Endian) for F280013x/F280015xdevices.
- u32ApiCompilerVersion – Version
number of the Code Composer Studio code generation tools used to compile the
API
Return Value
- Fapi_LibraryInfoType
(gives the information retrieved about this compile of the API)