SPRUJC5 April 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1
This reference guide provides a detailed description of the Texas Instruments TMS320F28P55x Flash API Library (FAPI_F28P55x_EABI_v4.00.00.00 & FAPI_F28P55x_COFF_v4.00.00.00) functions that can be used to erase, program and verify Flash on TMS320F28P55x devices. Even though the library names for TMS320F28P55x are different, the Flash API libraries are same. Note that the Flash API V4.00.XX.XX should be used only with TMS320F28P55x devices. The Flash API Library for TMS320F28P55x is provided in C2000Ware at C2000Ware_x_xx_xx_xx\libraries\flash_api\f28p55x.