Flash is an electrically erasable/programmable non-volatile memory that can be programmed and erased many times to ease code development. Flash memory can be used primarily as a program memory for the core, and secondarily as static data memory. This guide describes the usage of the flash API library to perform erase, program and verify operations for the on-chip Flash memory of F29H85x devices.
Arm® is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
All trademarks are the property of their respective owners.
This reference guide provides a detailed description of Texas Instruments' F29H85x Flash API Library (F29H85x_NWFlashAPI_v21.00.00.00.lib) functions that can be used to erase, program and verify Flash on F29H85x devices. Note that Flash API v21.00.00.00 should be used only with F29H85x devices. The Flash API Library is provided in the F29H85x SDK at "f29h85x-sdk > source > flash_api"